AXIS#.SENSORLESS.BW

Description

Returns the actual bandwidth of the Sensorless Field-Oriented Control (SFOC) in RPM limited by the maximum velocity of the motor and maximum allowed commutation frequency (599Hz). This bandwidth can be set using AXIS#.SENSORLESS.BWU.


  • To convert the bandwidth to Hz, use the following equation:
    AXIS#.SENSORLESS.BW [Hz] = AXIS#.SENSORLESS.BW [RPM] x AXIS#.MOTOR.POLES / 120

Versions

Action Version Notes
Implemented 02-03-03-000

 

General Information

Type

Read Only

Description Reads the SFOC bandwidth

Units

rpm

Data Type

Float

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.SENSORLESS.BW

5018h

07h

Signed32

-

1000:1

Read only

No

AXIS2.SENSORLESS.BW

5118h

07h

Signed32

-

1000:1

Read only

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

7401

1

7401 (0x1ce9)

AXIS1.SENSORLESS.BW

Signed32

Read Only

Yes

72937

2

7401 (0x1ce9)

AXIS2.SENSORLESS.BW

Signed32

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.SENSORLESS.BW

7401

Float

Read Only

-